Below are answers to popular Food Waste Disposer and Steaming Hot Water tap questions. For further assistance, please click here
Food waste is fed into the disposer together with water from the ambient cold tap. The food waste is simply and quickly ground into fine particles, no knives and no blades. The food waste is then flushed through the waste disposer and into your normal waste system. The InSinkErator food waste disposer is designed to cope with most types of food waste, including small bones, meat, fish, peelings, eggshells, nuts and much, much more.
Only a few seconds, although it depends on the quantity and type of waste. The sound of the disposer will change, when there is no longer any food waste in the grind chamber and the impellers spin freely. After all food waste is ground, turn off the disposer and let the water run for about 15 seconds to flush the waste out of the grind chamber and out to the water drainage/sewer pipes. Only a small amount of water, time and effort is required.
Waste disposers are built to rigorous standards on electrical and appliances. Contrary to what some may think, they do not have knives or blades…an assumed cause of safety concern.
Most forms of food waste can be put through the food waste disposer — bones from fish and poultry, meat, large meat bones, fish scraps, vegetables, fruit, egg shells, and much more. Very stringy or fibrous foods such as celery should be avoided. Food waste disposers are designed for food waste only and packaging materials should not be put into the disposer.
There are 4 easy steps to operate a disposer:
*Never pour grease or fat into disposer or any drain.
No. InSinkErator disposers are designed to be maintenance-free. Regular usage is the best way to keep your disposer in good condition. A moderate stream of ambient cold water following each use will keep your disposer clean.
InSinkErator steaming hot water taps connect to mains ambient cold water. You can carry out the work yourself, or use a plumber if you prefer. See installation guide.
No. Your hot water tap can be installed into your existing sink.
Based on average family usage, you can expect to change the filter on your InSinkErator steaming hot water tap twice a year.
All InSinkErator steaming hot water taps use the space saving 2.5 litre tank which sits neatly under most sinks.
No, no servicing is necessary.