The InSinkErator Experience….

Simple To Use And Great For The Environment


Food waste disposers have a come long way since the 80’s, they are quieter and more powerful than ever before. 

Not only do they offer a simple and convenient solution to managing food waste in your home, but they are also great for the environment.

Read More...

How does a food waste disposer work?

How does a food waste disposer work?

MYTH BUSTING

Today’s modern InSinkErator Food Waste Disposers are a far cry from the disposers of the early 80’s. The technology has come a long way, and this is testament to our commitment to continually improving the concept we invented over 75 years ago. Yet there are some myths that exist so let’s look at those now.

InSinkErator Evolution 250 Food Waste Disposer
Let's talk environment

Let's talk environment

Ground food scraps are sent via household plumbing to the sewerage system instead of to landfill which is not an environmentally responsible solution. At capable treatment plants methane may be captured from ground food waste and recycled into renewable energy

The noisy disposer is a thing of the past

The noisy disposer is a thing of the past

The days of the roaring disposer beneath the sink are gone with the Evolution Series® disposer. We remember when you needed to shout over them to be heard. Not anymore. These new units feature an Anti-vibration mount®, Multi-Layer® sound insulation and a noise reducing sink baffle that reduces the noise coming up through the sink opening.

Cheap as chips to run

Cheap as chips to run

InSinkErator Food Waste Disposers are very energy efficient costing less than $3.50 to run in electricity per year.

Minimal water

Minimal water

Food waste disposers are low in water usage, using less than 1% of the total household water consumption. This is the equivalent to approximately one toilet flush per day

Guess what they can grind

Guess what they can grind??

While InSinkErator Food Waste Disposers are ideal for disposing of fruit and veggie scraps they also eliminate bones, seafood, meat products, dairy, coffee grounds and much more. Evolution 200 can grind practically all food waste and is ideal for more challenging food scraps such as stringy vegetables.

Not a blade in sight

Not a blade in sight

InSinkErator Food Waste Disposers do NOT contain blades. Instead, they have small lugs on a spinning plate that act like a hammer effect breaking down the food. Once small enough the food waste is then passed through the small holes in a stationary grind ring and passes into the sewerage system.


Unlike a bin they never need emptying

Unlike a bin they never need emptying

An InSinkErator Food Waste Disposer fits to your existing plumbing under your kitchen sink therefore never needs emptying. After food is ground it travels through the sewerage system to a wastewater treatment plant just as the waste from the toilet would for treatment. Remember you can retro fit a disposer if it is not installed at the time of build



Evolution Series

Experience the Evolution Difference

If you are after the least amount of noise and the ability to grind more challenging food scraps such as stringy vegetables, you should look at the Evolution Series™. All are quiet, particularly Evolution 200 and 250, which also offers the finest grind. These are our superior models and offer the end user an ideal in-home experience.

Read More...
Experience the Evolution Difference
M Series

Standard Range

If you are looking for basic grinding technology, and sound is not a factor, then Models 46 or 56 deliver strong, reliable performance. Model 66 and E75 are the most powerful of the standard M Series and can grind most food scraps efficiently, making waste disposal quick and easy.

Read More...
Standard Range
Commercial Food Service

Reduces food waste as well as it reduces inefficiency.

Food waste that decomposes in skip bins creates odours, attracts pests and serves as a breeding ground for bacteria. Disposers help keep food waste out of skip bins. They also reduce staff trips to the skip bins and waste-hauling costs while increasing kitchen efficiency and profitability. Bottom line? Food waste disposers play an important role in saving your operation money. .

Read More...
Reduces food waste as well as it reduces inefficiency.
Please enable JavaScript to use this website.