h003-food-waste-disposer

Operating and Troubleshooting


If the Disposer is not working?

  1. Check:
    • Electric Switch is on
    • Air switch is on
  2. If the disposer is still not working:
    • Reset the trip switch as below
  3. If the disposer is running but making weird noise:
    • Check if there is any non-food object inside the disposer (eg: spoon, etc)
    • Remove the object using hand or tongs

If the above steps don’t solve the problem, contact your supplier for service support

Read More...
If the Disposer is not working?
If the Disposer is not working?

Things to be cautious about the Disposer


  • DON’T pour grease, oil or fat (oil from unwashed dishes or left over plate is ok)
  • DON’T put non-food material into the disposer
  • DON’T use hot water when grinding food waste
  • DON’T turn off water or disposer until grinding is completed
  • DON’T fill disposer with a lot of food waste all at once
  • DON’T insert hands or fingers into disposer before switching off the disposer

What can I grind?







Please enable JavaScript to use this website.