The Top 10 Christmas Food Recipes according to TikTok


The festive season is nearly upon us! With searches for ‘Christmas recipes’ up by 314% in the last month, people are searching for what they can cook this Christmas.


TikTok users have been sharing their favourite Christmas dishes. With the hashtag ‘#christmasrecipes’ receiving over 164 million views on TikTok, InSinkErator have revealed the top 10 festive recipes according to TikTok.


tik-tok-xmas


Expert, Jamie Griffin from InSinkErator said: “As we approach the most highly anticipated time of the year, food is the one of the largest elements of the festive season that people look forward to.


With many people overbuying when it comes to their Christmas food shop, TikTok gives users great pointers in terms of what to buy and what Christmas recipes you can follow to ensure that nothing goes to waste.”


Top 10 Christmas Recipes according to TikTok


Ranking

                 Recipe

Views

1

Christmas Crack

13,300,000

2

Baked Brie

4,000,000

3

Christmas Apple Pie

3,100,000

4

Garlic Butter Roast Potatoes   

2,900,000

5

Cinnamon Christmas Trees

2,100,000

6

Iced Hot Chocolate

1,400,000

7

Beetroot Cured Salmon

1,300,000

8

Chicken Pot Pie

885,800

9

Nutella Christmas Tree

644,700

10

Cranberry Jalapeno Dip

523,000


1. Christmas Crack - 13.3 million views

@biggirlbakery has gone viral on TikTok, receiving over 13.3 million views, after she revealed how to make her favourite Christmas recipe, Christmas Crack. With the hashtag ‘#christmascrack’ receiving 49.6 million views, it comes as no surprise that TikTok users are loving this recipe.


In order to create your own Christmas Crack, simply melt butter and brown sugar on a medium heat until the sugar is fully dissolved. Then line a baking sheet with parchment paper and line as many salted crackers as you can onto the sheet.


Pour the butter and sugar mixture over the crackers and place in a 400 degree oven for 6 minutes, advises @biggirlbakery. Remove from the oven and then cover with chocolate chips. Spread the melted chocolate and add any toppings you like. Wait to cool and enjoy!


Jamie Griffin from InSinkErator comments: “This is an extremely simple and cost effective recipe to enjoy throughout the festivities. Utilising food products you may have in your cupboards and also using fresh produce which may have a shorter shelf life, it is the perfect way to make use of what you may already have.”


2. Baked Brie - 4 million views

Receiving over 4 million views on TikTok, baked brie appears to be a necessity for winter and the festive season. @yesidothecooking went viral on TikTok after she revealed her perfect baked brie Christmas recipe.


Simply top baked brie with fig jam, walnuts, rosemary, honey and olive oil. Bake it in the oven until the cheese is soft and then drizzle with honey and sprinkle some salt on top.


Jamie Griffin from InSinkErator comments: “This is a simplistic yet delicious recipe which is perfect for the festivities. With cheese being named as one of the most common food items that Brits tend to waste, this is the ideal recipe to ensure that this isn't the case. With cheese boards being extremely common around Christmas time, this recipe is the perfect way to differentiate your cheese board.


The options are endless when it comes to toppings. Food products including chilli and cranberry would be a brilliant addition to brie and could minimise festive food wastage. Dipping cheeses like brie also allow you to use any leftover bread rather than it going to waste.”


3. Christmas Apple Pie - 3.1 million views


@absolutechristmas has received over 3.1 million views on TikTok, after showcasing their Christmas Apple Pie recipe.


With the ingredients including dough, pie crust ,flour, sugar, salt, butter, and egg wash as well as apples, lemons, cinnamon, cardamom and vanilla bean paste for the filling. It is the perfect recipe for the winter months which everyone will enjoy.


Jamie Griffin from InSinkErator says: “With fresh fruit being one of the most commonly wasted food items, recipes like @absolutechristmas’ apple pie allows such food waste products to be used as ingredients to make homemade recipes. This festive dish is extremely versatile as you can alter the recipe in order to fill your pie with suitable ingredients which may be close to their use by date, whether that be berries or even something savoury.”


4. Garlic Butter Roasted Potatoes - 2.9 million views


Some may say that roast potatoes are the best part of Christmas dinner. @thegrubworkskitchen has received a staggering 2.9 million views after revealing his roast potato recipe on TikTok. Showcasing his golden crispy potatoes coated in a sage garlic butter, @thegrubworkskitchen says all you need to buy is potatoes, stock, butter, garlic, sage and salt.


Simply peel and slice your potatoes and then bring to boil after adding your stock and salt. Boil until fork tender and then drain and allow to stand for 5 minutes. Cover the roasting tray with oil and place into a preheated oven for 15-20 minutes. Ensure to not add the potatoes straight into the oil.


Add your potatoes and coat in the oil and roast for 1 hour. Then melt your butter with sage and garlic on a medium heat. Let the butter infuse into the potatoes for 1-2 minutes and then roast your potatoes in some of the butter for the last 5 minutes.


Jamie Griffin from InSinkErator says: “This recipe will most definitely add something else to a traditional Christmas dinner. It utilises long life food products which have multiple uses. With potatoes being one of the most versatile foods you can buy when it comes to food shopping, you can use any excess for other meals/recipes whether they be festive or not.”


5. Cinnamon Christmas Trees - 2.1 million views


When it comes to Christmas time, a sweet baked treat is at the forefront of many minds. @annykaly has received over 2.1 million views after posting her cinnamon Christmas tree recipe. According to @annykaly, all you need is a puff pastry sheet, butter, brown sugar, cinnamon, egg wash, powdered sugar and skewers.


Jamie Griffin from InSinkErator says: “This recipe has taken off on TikTok and it comes with no surprise that @annykaly has received over 2 million views. This is the ideal cost effective sweet treat for the festive season which everyone will enjoy. When it comes to the filling, the options don’t end with cinnamon, other TikTok videos have showcased the use of nutella and other delicious sweet condiments.”

Please enable JavaScript to use this website.