INSINKERATOR® PARTICIPATES IN A ONE OF A KIND SUSTAINABLE HOUSING PROJECT


We supplied our food waste disposers to a unique, innovative and sustainable housing development, Oceanhamnen in Helsingborg, Sweden. Consisting of approximately 350 residential apartments and three office buildings, as part of the first stage, Oceanhamnen aims to be an economically, environmentally and socially sustainable urban development. When complete, the development is estimated to boast 1,200 residential apartments and 40,000 square metres of office and hotel space, which will also include shops and local services such as a dentist and GP surgery.


A major aspect of the project is its new and unique sewerage system, which collects waste through three separate wastewater streams. We provided Oceanhamnen residents with an Evolution 100 food waste disposer to direct their food waste to RecoLab, a specially designed wastewater treatment facility, to support a project aim of reducing greenhouse gases in the area by 50 per cent. Not only does collecting food waste in this way reduce greenhouse gas formation in landfill, the nutrients from the food waste can also be recovered and turned into biogas and fertiliser. Furthermore, by installing an InSinkErator® food waste disposer into every apartment means that residents of Oceanhamnen don’t have to handle smelly, unhygienic food waste, or have it lingering in their kitchen.


Through an independent survey conducted for NSVA (Nordvästra Skånes Vatten och Avlopp/North West Scania Water and Waste Water) with residents of the sustainable housing project, InSinkErator® found that nearly all of those questioned (96 per cent) would choose to own a food waste disposer again. Furthermore, 93 per cent would recommend the product to others and 79 per cent are enthusiastic and proud to show visitors their food waste disposer. 70 per cent of those surveyed are satisfied with using a food waste disposer, compared to the alternative of collecting waste in paper bags and taking it to the basement of the building.


InSinkErator Oceanhamnen Case Study se

(Photography credit: Helsingborgs stad, David Lundin)

Click here to view video on Oceanhamnen.


Hamse Kjerstadius, Development engineer, NSVA, says: “Present day sewerage systems are not built for recovery, they are built to remove nutrients and they do that very well, however, the systems that we have installed in Oceanhamnen are actually designed to recover products from wastewater.


“The main advantage is the separation of flows with a high concentration of nutrients and organic matter (food waste and sewage). Once we have separated them, we can apply much better technology at the treatment plant. And that’s the reason why we can increase the nutrient recovery so much.”


Anne Kaarlela, Marketing Communications and Customer Service Manager, Europe, InSinkErator® says: “We are thrilled to be part of the Oceanhamnen project, providing residents with a hygienic and sustainable solution to managing their food waste, while also ensuring the food waste generates biogas instead of producing methane in landfill. It’s important to us at InSinkErator® to participate and support projects that aim to enhance consumers’ lives through innovative, sustainable developments and we hope that the positive outcomes from the Oceanhamnen project influence and encourage future sustainable housing developments.”


We  currently has a healthy inventory and are committed to keeping our retail partners fully stocked up with their chosen InSinkErator® products.


For more information on sustainable products from InSinkErator®, please consult your Account Manager.

Please enable JavaScript to use this website.