InSinkErator® shortlisted in the Livingetc Style Awards


InSinkErator® has been shortlisted as a finalist for two awards - the ‘Home Tech and Appliance’ and ‘Kitchen Fittings’ categories at the first-ever Livingetc Style Awards 2021, for its must have eco-gadget Evolution 250 Food Waste Disposer and Italian designed and manufactured premium styled 4N1 Touch Taps.


As the UK’s most influential contemporary homes brand, Livingetc’s new awards programme will celebrate the finishing touches that makes homes original. With a network of over 300,000 monthly global users and over 1.4m social fans, receiving a Livingetc Style Award gives brands a competitive edge through high consumer exposure and endorsement.


The InSinkErator® Evolution 250 Food Waste Disposer, nominated for the Home Tech and Appliances Award is a must have eco-gadget for the home. Cooking from scratch at home becomes instantly more hygienic, when an Evolution 250 is installed, as inedible food scraps can be disposed of within seconds. It’s a sustainable kitchen appliance that is designed to fit easily under all sinks, offering an easy, safe and practical solution to managing food waste in the home, especially where home composting is not possible, eliminating the need for consumers to use an unhygienic food waste caddy.


The stylish and innovative InSinkErator® 4N1 Touch Taps are shortlisted for the Kitchen Fittings Award; these combination taps boasts solid, premium, low lead brass composition, offering extended reliability. The 4N1 dispenses instant filtered cold water, via unique touch button control, and instant filtered steaming hot water as well as regular hot and cold water, from the same combined fixture. Streamlining kitchen worktops, the InSinkErator® 4N1 Touch tap removes the need for multiple kitchen taps, kettles and water filter jugs while offering consumers an elegant alternative to buying an endless amount of single-use, plastic, bottled water, therefore decluttering the kitchen and reducing plastic waste.


ISE_Living_1180x664_image website


The Livingetc Style Awards will be judged by a panel of industry experts and tastemakers, including respectable names such as Lucinda Chambers, Fashion Director at British Vogue and Luxury Interior and Design Journalist Sarah Spiteri. Winners will be announced in June and will have the opportunity to be featured across Livingetc’s large online and print platforms.


Anne Kaarlela, Marketing Communications and Customer Service Manager Europe and Russia InSinkErator®, says:

“We’re absolutely delighted to be shortlisted as a finalist for not one but two awards at the Livingetc Style Awards for our sustainable Evolution 250 Food Waste Disposer and premium 4N1 Touch Tap. We look forward to the winners being announced later this June”.

Please enable JavaScript to use this website.