The InSinkErator 4N1 Touch combination tap has gained approval from the Water Regulations Advisory Scheme (WRAS).

The approval from WRAS demonstrates the commitment of InSinkErator to compliance and the safety of its consumers, by encouraging the efficient use of water within the home and offering products that prevent the contamination of public water supplies. By achieving WRAS approval, the 4N1 Touch tap also meets the necessary regulations of the national water suppliers to be installed into new-build homes. The WRAS approved 4N1 Touch tap comes complete with an InSinkErator NeoTank and filter unit that also carries the WRAS approval, meaning the complete unit boasts this accreditation.

Designed to meet the increased consumption of filtered drinking water, the InSinkErator 4N1 Touch provides a stream of filtered cold water for 30 seconds, at the touch of a button. The 4N1 also safely dispenses filtered steaming hot water, alongside regular hot and cold water from the same combined fixture, removing the need for multiple kitchen taps, kettles and water filter jugs.

Marco Pastore, Product Manager, Europe and Russia InSinkErator, says: “We are delighted that the complete range of 4N1 Touch taps has achieved the approval from the Water Regulations Advisory Scheme. It is an important accreditation for us at InSinkErator as well as for our trade partners when specifying a specialist kitchen tap. For further peace of mind, our WRAS approved 4N1 Touch taps also benefit from a five-year in-home limited warranty on the tap and two-year parts and labour limited warranty on the tank.”

The InSinkErator 4N1 Touch is available in three shapes, L, J or U, complementing a variety of kitchen styles. All three 4N1 Touch shapes are available in traditional finishes of Brushed Steel or Polished Chrome as well as the on-trend finish of Velvet Black. A stylish, affordable combined fixture; the 4N1 Touch is designed and made in Italy with a solid, premium, low lead brass composition, adding extended reliability.

Please enable JavaScript to use this website.