Northern Ground - Buying Tips - Hero

Garburators are Septic-Safe

Despite common myths, InSinkErator® food waste disposers are a complement to your septic system.

You've probably been told that using a disposer to get rid of food waste is going to upset that delicate system. The reality is, it won't.

A garburator grinds food waste to easily flow through a home's plumbing and into a septic tank. Once there, food scraps decompose faster than other waste sent into the tank. Because food scraps are 70% to 90% water, they add very little to the solids that settle at the bottom of the tank. Studies show that septic systems attached to a garbage disposal don't require more frequent pumping than those that aren't.[1]


[1] Study of food waste degradation in a simulated septic tank - Hongjian Lin, Yuchuan Wang, Leif van Lierop, Carlos Zamalloa, Casey Furlong, Michael Keleman, Bo Hu, 2019

Read More...
You've probably been told that using a disposer to get rid of food waste is going to upset that delicate system. The reality is, it won't.
Northern Ground - Buying Tips - Hero
header_reducingfoodwaste

Reducing Food Waste

Want to know how you can reduce the negative impact of food waste on the environment?

Please enable JavaScript to use this website.