INSINKERATOR® 4N1 TOUCH TAP RECOMMENDED BY RUSTED REVIEWS


Our 4N1 Touch tap has been awarded the highly coveted Trusted Reviews ‘Recommended’ accolade, achieving a high four and a half out of five star rating1.


Trusted Reviews is an independent product testing online publication, providing readers with unbiased views and advice on the latest technology and gadgets available to consumers in the UK. The Trusted Reviews team were impressed with the design and convenience offered by the 4N1 Touch tap, with the reviewer commenting, ‘I love the all-in-one design of this tap, giving everything from boiling water and regular hot and cold to filtered water without cluttering the sink’1.


With sustainability being an important factor that consumers consider when purchasing a new item for their home, the team also measured the energy used by our NeoTank to heat the water. Trusted Reviews commended the combination tap for its efficiency when compared to using a kettle to boil water, which is often then re-boiled throughout the day, resulting in additional energy consumption. The team also noted that ‘you only take out as much water as you need, so only a little energy is needed to top up the tank’s temperature1’, further highlighting the tap’s sustainable credentials.  

MicrosoftTeams-image (14)


Designed for consumers at all life stages, the review also describes how the 4N1 Touch is safe to use, thanks to the self-closing, easy to grip, hot water handle with a push-lever safety locking mechanism. This ensures that the flow of water stops immediately after the lever is released, eliminating the risk of leaving steaming hot water running.


Anne Kaarlela, Marketing Communications and Customer Service Manager, Europe and Russia, InSinkErator®, says:


“We are thrilled that our 4N1 Touch tap has received the ‘Recommended’ accolade by Trusted Reviews. It’s important to us at InSinkErator® that our products are not only stylish, but that they enhance the user’s home life, in terms of convenience as well as offering resource savings too. In addition to highlighting its numerous benefits, we hope Trusted Reviews’ unbiased recommendation can support our trade partners when encouraging their customers to invest in an InSinkErator® 4N1 Touch tap.”


The 4N1 Touch tap offers instant filtered steaming hot water, instant filtered ambient cold water and regular hot and cold water from one combined fixture. It is available in three different shapes; L, J or U, to complement a variety of kitchen styles. All three 4N1 Touch shapes are available in traditional finishes of Brushed Steel or Polished Chrome, as well as the on-trend finish of Velvet Black.


For more information on the 4N1 Touch tap, please contact your Account Manager.


References:

1 https://www.trustedreviews.com/reviews/insinkerator-4n1-touch



Please enable JavaScript to use this website.